5G NR
Remote Command - Full-filled Config
User Interface - Full-filled Config
|
SCPI Command |
[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:CONFig:FFILled "Bandwidth: FR1BW5M|FR1BW10M|FR1BW15M|FR1BW20M|FR1BW25M|FR1BW30M|FR1BW35M|FR1BW40M|FR1BW45M|FR1BW50M|FR1BW60M|FR1BW70M|FR1BW80M|FR1BW90M|FR1BW90M|FR1BW100M|FR2BW50M|FR2BW100M|FR2BW200M|FR2BW400M|FR2BW800M|FR2BW1600M|FR2BW2000M, Numerology: MU0|MU1|MU2Ncp|MU2Ecp|MU3|MU5|MU6, Modulation: PIBPsk|QPSK|QAM16|QAM64|QAM256|QAM1024, OFDMType: DFTS|CP, RBNumberRestriction: ON|OFF, DuplexType: FDD|TDD, SlotConfigurationPeriod: MS0P5|MS0P625|MS1|MS2|MS1P25|MS2P5|MS5|MS10, NumberOfDownlinkSlots:<integer>, NumberOfDownlinkSymbols: <integer>, NumberOfUplinkSlots:<integer>, NumberOfUplinkSymbols: <integer>" |
|
SCPI Example |
RAD:NR5G:WAV:CCAR:CONF:FFIL "Bandwidth: FR1BW90M, Numerology: MU1, DuplexType: TDD, Modulation : QAM16, SlotConfigurationPeriod: MS5, NumberOfDownlinkSlots: 5, NumberOfDownlinkSymbols: 4, NumberOfUplinkSlots: 5, NumberOfUplinkSymbols: 3" |
|
Couplings |
Parameters and default values of Full Filled Config are listed below: Bandwidth: FR1BW100M Numerology: MU1 Modulation: QPSK OFDMType: CP RBNumberRestriction: OFF DuplexType: FDD SlotConfigurationPeriod: MS5 NumberOfDownlinkSlots: 7 NumberOfDownlinkSymbols: 6 NumberOfUplinkSlots: 2 NumberOfUplinkSymbols: 4 One combined string is needed to be inputted in SCPI command. The format of it is "name: value , name: value …" . Default value will be used if parameter is not provided. The order of parameters does not matter. Parameter's name and value are case sensitive. If parameter's name is incorrect, error " -224, "Illegal parameter value; xxx is incorrect parameter name." will be generated. If parameter's type is enum and the inputted enum value is illegal , error " -224, Illegal parameter value; xxx has incorrect value." will be generated. |
|
Notes |
In A.10.00, Modulation=QAM1024 is available when carrier type is downlink. |
|
Initial S/W Revision |
A.09.00 |
|
Modified S/W Revision |
A.10.00, A12.00 |
|
GUI Location |
Apps > 5G NR > Carrier > Full-filled Config |
|
Initial S/W Revision |
A.01.00 |
|
Modified S/W Revision |
A.09.00, A.10.00, A.12.00 |
Choices:
Downlink: Based on the Table 5.3.2-1 and 5.3.2-2 in 38.104
Uplink: Based on the Table 5.3.2-1 in 38.101-1 and 38.101-2
Selects the bandwidth configuration for the carrier.
Selects the numerology of the
Choices: TDD | FDD
Selects the duplex type.
When TDD is selected, several TDD parameters appear below. These TDD parameters are reset to default values whenever numerology changes or FR changes. (The default values are different for each numerology.)
Sets the periodicity of DL-UL pattern. The choices are related to numerology.
Sets the number of consecutive full DL slots at the beginning of each DL-UL pattern. The range is related to the numerology and slot configuration period.
Range: 0 ~ 14 for Normal CP; 0 ~ 12 for Extended CP
Sets the number of consecutive DL symbols in the beginning of the slot following the last full DL slot.
Sets the number of consecutive full UL slots at the end of each DL-UL pattern. The range is related to the numerology and slot configuration period.
Range: 0 ~ 14 for Normal CP; 0 ~ 12 for Extended CP
Sets the number of consecutive UL symbols in the end of the slot preceding the first full UL slot.
Displays the number of special slots.
Displays the TDD slot allocation for one period.
Choices: DFT-s-OFDM | CP-OFDM
Select the OFDM Type for uplink.
Choices:
Downlink Carrier: QPSK | 16QAM | 64QAM | 256QAM
Uplink Carrier: pi/2 BPSK | QPSK | 16QAM | 64QAM | 256QAMQPSK
Select the Modulation type to be configured for current carrier.